Neutral-Grounding-Resistor Monitor Set-Point Assistant
NGR Monitor Set-Point Assistant
This assistant provides set-point recommendations for Littelfuse Startco SE-325, SE-330, SE-330AU, and SE-330HV Neutral-Grounding-Resistor Monitors.
Open the NGR Monitor Set-Point Assistant
Motor and Feeder Protection Online Demos
Virtual FPU-32 (VFPU)
450
450
Virtual FPU-32 (VFPU)
VFPU is a "virtual" FPU-32 Feeder Protection Unit that allows the user to scroll through the menus.
Open the Virtual FPU-32
Virtual MPS (VMPS)
810
460
Virtual MPS (VMPS)
VMPS is a "virtual" MPS-OPI Operator Interface that allows the user to scroll through the menus.
Open the Virtual MPS
Virtual MPU-32 (VMPU)
450
450
Virtual MPU-32 (VMPU)
VMPU is a "virtual" MPU-32 Motor Protection Unit that allows the user to scroll through the menus.
Open the Virtual MPU-32
MPU-32 Tutorial
800
553
MPU-32 Tutorial
This tutorial covers basic topics in using the MPU-32 Motor Protection Unit, including how to enter set points, how to view metered information, and how to handle trips and alarms. Step-by-step instructions guide you through every button press as you accomplish the task at hand.
Open the MPU-32 Tutorial
Symmetrical Component Calculator
Symmetrical Component Calculator
This calculator finds the unbalance of three-phase input quantities using the positive- and negative-sequence component method. It can be used in conjunction with relay test equipment to verify the unbalance readings for the Littelfuse Startco FPU-32, MPU-32, and MPS.
Download Symmetrical Component Calculator v1.0