Littelfuse offers a broad range of TVS diodes, including high peak pulse current and peak pulse power options up to 10kA and 30kW respectively. Littelfuse backs our products with over 80 years of circuit protection expertise and application knowledge developed by working with our industry-leading customers. You can learn more about our range of tvs diode products by viewing our Circuit Protection Product Selection Guide.
The Transient Voltage Suppressor diode (also known as a TVS Diode) is a protection diode designed to protect electronic circuits against transients and overvoltage threats such as EFT (electrically fast transients) and ESD (electro-static discharge). TVS Diodes are silicon avalanche devices typically chosen for their fast response time (low clamping voltage), lower capacitance and low leakage current. Littelfuse TVS diodes are available in both uni-directional (uni-polar) or bi-directional (bi-polar) diode circuit configurations.
When selecting TVS Diodes there are some important parameters to be considered, these are; Reverse Standoff Voltage (VR), Peak Pulse Current (IPP) and Maximum Clamping Voltage (VC max). View the Circuit Protection Product Selection Guide to learn more about how to select these devices and Littelfuse’s complete TVS diode offering
What are TVS Diodes?
TVS Diodes are electronic components designed to protect sensitive electronics from high-voltage transients. They can respond to overvoltage events faster than most other types of circuit protection devices, and are offered in a variety of surface mount and through-hole circuit board mounting formats.
They function by limiting voltage to a certain level (referred to as a "clamping" device) with p-n junctions that have a larger cross-sectional area than those of a normal diode, allowing them to conduct large currents to ground without sustaining damage.
TVS Diodes are generally used to protect against electrical overstress such as those induced by lightning strikes, inductive load switching, and electro-static discharge (ESD) associated with transmission on data lines and electronic circuits.
Littelfuse TVS Diodes can fit a wide range of circuit protection applications but were primarily designed to protect I/O interfaces in telecommunication and industrial equipment, computers and consumer electronics.
Littelfuse TVS Diode characteristics include:
- Low incremental surge resistance
- Unidirectional and Bidirectional polarities available
- Reverse standoff voltages range from 5 to 512V
- RoHS compliant–Matte Tin Pb-free plated
- Surface-mount power ratings from 400W to 5,000W
- Axial lead power ratings from 400W to 30,000W (30kW)
- High current protection available for 6kA and 10kA
For insight about other Transient Suppression Technologies and how they compare, please refer to Littelfuse Application Note AN9768.
Littelfuse TVS Diode Product Selection Table
TVS Diodes are used to protect semiconductor components from high-voltage transients. Their p-n junctions have a larger cross-sectional area than those of a normal diode, allowing them to conduct large currents to ground without sustaining damage. Littelfuse supplies TVS Diodes with peak power ratings from 400W to 30kW, and reverse standoff voltages from 5V to 495V.
You can get additional TVS Diode selection guidance by visiting the TVS Diode definition and selection page by clicking here
Series Name and Page Link |
Package Type |
Reverse Standoff Voltage (VR) |
Peak Pulse Power Range2 (PPP) |
Peak Pulse Current
(IPP 8x20μs) |
Operating Temperature |
Surface Mount - Standard Applications (400-5000W): |
SMAJ |
DO-214AC |
5.0-440 |
400W |
Not Applicable |
-85° to +302° F
(-65° to +150° C) |
P4SMA |
DO-214AC |
5.8-495 |
400W |
SACB |
DO-214AA |
5.0-50 |
500W |
SMBJ |
DO-214AA |
5.0-440 |
600W |
P6SMB |
DO-214AA |
5.8-495 |
600W |
1KSMB |
DO-214AA |
5.8-136 |
1000W |
SMCJ |
DO-214AB |
5.0-440 |
1500W |
1.5SMC |
DO-214AB |
5.8-495 |
1500W |
SMDJ |
DO-214AB |
5.0-170 |
3000W |
5.0SMDJ |
DO-214AB |
12-170 (uni-directional)
12-45 (bi-directional) |
5000W |
Axial Leaded - Standard Applications (400-5000W): |
P4KE |
DO-41 |
5.8-495 |
400W |
Not Applicable |
-85° to +302° F
(-55° to +175° C) |
SA |
DO-15 |
5.0-180 |
500W |
SAC |
DO-15 |
5.0-50 |
500W |
P6KE |
DO-15 |
5.8-512 |
600W |
1.5KE |
DO-201 |
5.8-495 |
1500W |
LCE |
DO-201 |
6.5-90 |
1500W |
3KP |
P600 |
5.0-220 |
3000W |
5KP |
P600 |
5.0-250 |
5000W |
Axial Leaded - High Power: |
15KPA |
P600 |
17-280 |
15000W |
Not Applicable |
-85° to +302° F
(-55° to +175° C) |
20KPA |
P600 |
20.0-300 |
20000W |
30KPA |
P600 |
28.0-288 |
30000W |
AK6 |
Radial Lead |
58-430 |
NA |
6000A |
-67° to +347° F
(-55° to +150° C) |
AK10 |
Radial Lead |
58-430 |
NA |
10000A |
Automotive Applications: |
SLD |
P600 |
10-24 |
2200 based on 1μs/150ms pulse |
NA |
-85° to +302° F
(-65° to +175° C) |
- Detailed information about most product series listed here can be found clicking on the series name in the far left column.
- For Maximum Clamping Voltage (VC) please refer to electrical characteristics table within each series data sheet
- You can get additional TVS Diode selection guidance by perusing Littelfuse's Electronic Products Selection Guide.
- All products are Halogen Free
- All products are RoHS Compliant
Transient Threats – What Are Transients?
Voltage Transients are defined as short duration surges of electrical energy and are the result of the sudden release of energy previously stored or induced by other means, such as heavy inductive loads or lightning. In electrical or electronic circuits, this energy can be released in a predictable manner via controlled switching actions, or randomly induced into a circuit from external sources.
Repeatable transients are frequently caused by the operation of motors, generators, or the switching of reactive circuit components. Random transients, on the other hand, are often caused by Lightning and Electrostatic Discharge (ESD). Lightning and ESD generally occur unpredictably, and may require elaborate monitoring to be accurately measured, especially if induced at the circuit board level. Numerous electronics standards groups have analyzed transient voltage occurrences using accepted monitoring or testing methods. The key characteristics of several transients are shown in the table below.
|
VOLTAGE |
CURRENT |
RISE-TIME |
DURATION |
Lighting |
25kV |
20kA |
10 μs |
1ms |
Switching |
600V |
500A |
50 μs |
500ms |
EMP |
1kV |
10A |
20ns |
1ms |
ESD |
15kV |
30A |
<1ns |
100ns |
Table 1. Examples of transient sources and magnitude
Characteristics of Transient Voltage Spikes
Transient voltage spikes generally exhibit a "double exponential" wave, as shown below for lightning and ESD.
![](https://www.littelfuse.com/data/en/TVS_Site_Image/TVS_fig027.jpg)
Figure 1. Lightning Transient Waveform
![](https://www.littelfuse.com/data/en/TVS_Site_Image/TVS_fig028.jpg)
Figure 2. ESD Test Waveform
The exponential rise time of lightning is in the range 1.2μsec to 10μsec (essentially 10% to 90%) and the duration is in the range of 50μsec to 1000μsec (50% of peak values). ESD on the other hand, is a much shorter duration event. The rise time has been characterized at less than 1.0ns. The overall duration is approximately 100ns.
Why are Transients of Increasing Concern?
Component miniaturization has resulted in increased sensitivity to electrical stresses. Microprocessors for example, have structures and conductive paths which are unable to handle high currents from ESD transients. Such components operate at very low voltages, so voltage disturbances must be controlled to prevent device interruption and latent or catastrophic failures.
Sensitive microprocessors are prevelant today in a wide range of devices. Everything from home appliances, such as dishwashers, to industrial controls and even toys use microprocessors to improve functionality and efficiency.
Most vehicles now also employ multiple electronic systems to control the engine, climate, braking and, in some cases, steering, traction and safety systems.
Many of the sub- or supporting components (such as electric motors or accessories) within appliances and automobiles present transient threats to the entire system.
Careful circuit design should not only factor environmental scenarios but also the potential effects of these related components. Table 2 below shows the vulnerability of various component technologies.
Device Type |
Vulnerability (volts) |
VMOS |
30-1800 |
MOSFET |
100-200 |
GaAsFET |
100-300 |
EPROM |
100 |
JFET |
140-7000 |
CMOS |
250-3000 |
Schottky Diodes |
300-2500 |
Bipolar Transistors |
380-7000 |
SCR |
680-1000 |
Table 2: Range of device vulnerability.
Comparison to Other Diode Technologies:
Diode Class |
Application |
Remarks |
Conventional Diode, Rectifier |
Power Control |
Useful for "steering" high currents; converting AC to DC. Typically found in large packages such as TO-220. |
Zener Diode |
Power Control |
Useful for regulation of DC voltage in power supplies. Typically found in medium-size to large packages (Axial, TO-220). |
Silicon Avalance Diode (SAD), Transient Voltage Suppressor (TVS) |
Over-Voltage Protection |
Useful for protecting circuits exposed to high-energy events such as lightning surges or voltage transients from mechanical switching of electrical circuits (EFT). Typically found in medium-size packages (Axial, DO-214). |
Diode Array |
Over-Voltage Protection |
Diode Arrays fall into the more broad category of Silicon Protection Arrays (SPA), which are targeted for ESD protection. Typically found in small surface-mount packages (SOIC-8, SOT-23, SC-70, etc …) |
Shottky Diode |
Power Control |
Useful for high-frequency (HF) rectification required for switch-mode power supplies. |
Varactor Diode |
RF Tuning |
Only known application of diodes that takes advantage of the junction capacitance characteristic. |
Comparison by Operating Characteristic:
Diode Class |
Reverse Breakdown Voltage
(VBR, VZ) |
Capacitance (CJ) |
Remarks |
Conventional Diode, Rectifier |
800-1500V |
Very High |
AC to DC power conversion |
Zener Diode |
Up to 100V |
Medium to High |
DC power regulation |
Silicon Avalance Diode (SAD), |
Up to 600V |
Medium |
Lightning surge and voltage transient protection |
Diode Array |
Up to 50V |
Low (< 50pF) |
ESD protection of high-frequency data circuits |
Comparison by Device Construction:
A Schottky diode is formed by a metal to semiconductor junction. Electrically, it conducts by the majority carrier and possesses fast response with lower current-leakage and forward bias voltage (VF). Schottky diodes are widely used in high frequency circuits.
Zener diodes are formed by a heavily doped P-N semiconductor junction. There are two physical effects which can be referred to as a Zener state (Zener effect and Avalanche effect). Zener effect occurs when there is a low reverse voltage applied to the P-N junction which conducts due to quantum effect. Avalanche effect occurs when a larger than 5.5 Volts voltage applied reversely to the PN junction during which the generated electron-hole pair collide with the lattice. Zener diodes based on the Zener effect are widely used as voltage reference sources in electronics circuitry.
A TVS diode is formed by a specially designed P-N semiconductor junction for surge protection. The PN junction is usually coated to prevent premature voltage arcing during non conducting state. When there is a transient voltage event, the TVS diodes conducts to clamp the transient voltage using the Avalanche effect. TVS diodes are widely used as an over voltage circuit protection device in telecommunications, general electronics, and digital consumer markets for lightning, ESD, and other voltage transient protection.
SPA stands for Silicon Protection Arrays. It is an array of integrated PN junctions, SCRs, or other Silicon protection structures packaged in a multi-pin structure. The SPA can be used as a integrated solution for ESD, lightning, and EFT protection for telecommunications, general electronics, and digital consumer markets where multiple protection opportunities exist. For example, it can be used for HDMI, USB, and Ethernet port ESD protection.
TVS Diode Glossary
Clamping Device
TVS is a clamping device that limits voltage spikes by low impedance avalanche breakdown of a rugged silicon PN junction. It is used to protect sensitive components from electrical overstress generated by induced lightning, inductive load switching and electrostatic discharge.
Operating Temperature Range
The minimum and maximum ambient operating temperature of the circuit in which a device will be applied. Operating temperature does not allow for the effects of adjacent components, this is a parameter the designer must take into consideration.
Capacitance
The property of a circuit element that permits it to store an electrical charge. In circuit protection, the off-state capacitance is typically measured at 1 MHz with a 2V bias applied.
Reverse Standoff Voltage (VR)
In the case of a uni-directional TVS diode, this is the maximum peak voltage that may be applied in the 'blocking direction' with no significant current flow. In the case of a bi-directional transient, it applies in either direction. It is the same definition as Maximum Off-state Voltage and Maximum Working Voltage.
Breakdown Voltage (VBR)
Breakdown voltage measured at a specified DC test current, typically 1mA. Usually a minimum and maximum is specified.
Peak Pulse Current (IPP)
Maximum pulse current which can be applied repetitively. Usually a 10x1000μs double exponential waveform, but can also be 8x20μs, if stated.
Maximum Clamping Voltage (VC or VCI)
Maximum voltage which can be measured across the protector when subjected to the Maximum Peak Pulse Current.
Peak Pulse Power (PPP)
Expressed in Watts or Kilowatts, for a 1ms exponential transient (see figure 1, page 23) it is IPP multiplied by VCL.