As an example, in the toaster circuit below, the black or hot wire is shorted to the metal casing of the toaster. When the circuit closes, all or part of the current is channeled through the toaster frame and then the green ground wire. When sufficient current flows (typically 6 x 15 A = 90 A), the circuit breaker will open. A protection relay could be installed to detect currents as low as 5 mA, which would open the circuit breaker at a significantly lower level, hence, much quicker than the traditional circuit breaker.
Although the example above shows a solidly grounded single-phase circuit, the philosophy is the same on three-phase circuits discussed later. Relays and monitors are specifically designed to look for the leading initiators shown in Table 1 by detecting low-level changes in current, voltage, resistance or temperature.
What are some issues that cause a ground-fault relay to trip accidentally?
Harmonics and higher-frequency noise, especially at the third harmonic, can be present in an electrical system and appear as fault current. Electrical noise is a growing problem as more users utilize variable frequency drives, inverters, battery storage/UPS, and even LED lighting. To avoid nuisance trips, select a high-quality ground-fault relay that removes harmonic frequencies and other noise from its measurements.
What are the benefits of using a grounded system over an ungrounded system?
One of the major concerns of an ungrounded system is the risk of transient overvoltage. An intermittent or arcing ground fault can result in a buildup of voltage on the system, stressing and deteriorating insulation and resulting in voltages as much as 6 times higher than the nominal system voltage. Another benefit of a grounded system is the ease of locating a ground fault. Ungrounded systems do not provide a path for ground-fault current to flow on the first fault, so current-based solutions are not used to detect a fault. Instead, voltage-based solutions or insulation monitors are used to detect presence of the fault.
However, because the voltage on the faulted phase will be reduced throughout the entire system, locating the fault can be very difficult. Grounded systems can utilize current-based ground-fault relays to locate exactly where the fault is.
In terms of faults, how many kinds of faults can there be?
There are 3 different types of faults: phase to phase faults, three phase faults and ground faults. Phase to phase faults or “short circuits” are found within a device when an overloaded electrical current flows through a wire and burns it out. According to the Dunki-Jacobs textbook 95% of faults are ground faults, 4% are considered phase to phase faults, and 1% are considered three phase faults.
What do ground-fault relays do?
In electrical circuits, current returns to its source. A current-based ground-fault relay may look for ground-fault current in one of two ways: 1.) Zero sequence. Here, the relay looks at the phase conductors to ensure that all current coming from the source returns on those same conductors. If some of the current is returning to the source through a different path (usually ground), the ground-fault relay will detect this difference and, if it exceeds a pre-determined amount for a pre-determined amount of time, the ground-fault relay will operate. 2.) Direct measurement. A ground-fault relay can also read the current in the connection between the transformer neutral and ground (even with a neutral grounding resistor). A ground fault anywhere in the system will return current through this path.