The TSA141300 utilizes the Versa-Time circuitry in a unique arrangement that provides random start and a lockout delay in one small, rugged, inexpensive package. When connected as shown, the TSA141300 in a multiple unit situation, prevents all units from starting at one time with its random start feature. The TSA141300 also prevents the compressor from recycling rapidly which could result in a lock rotor condition. This lockout delay is initiated at the end of each operation of the compressor. A momentary loss of power would also initiate the lockout delay.
See datasheet for operation details.
Lockout Delay—prevents rapid recycling of compressor in air conditioning, refrigeration, and heat pump equipment
Random Start Delay—provides staggered start up of multiple units