background-waves

Series: ALT Alternating Relays

8-pin Plug-in Alternating Relay
Product Status| Activei
info
The ALT alternating relays are used to alternate between two loads. The ALT is commonly used in duplex pumping applications to balance the runtime of both pumps.

The ALT-S is used in single high-level float applications. When the float switch opens, the alternating relay changes state, forcing the other pump to run the next time the float closes. All ALT relays have a built-in debounce feature that prevents the relay from changing state if the switch or float contact bounces momentarily.

The ALT-X has an internal cross-connected relay and is used in dual high-level float applications. These floats are commonly referred to as lead and lag floats.

The pumps alternate as in the ALT-S version but the crossconnected relay configuration allows both pumps to run simultaneously when both the lead and lag floats are closed. These relays are also available with a built-in switch (SW option) that is used to manually force one of the pumps to run every time the float switch is closed. This is helpful when a pump has been removed for repair or for test purposes. In the case of the ALT-X-SW, the switch essentially forces one pump to be the lead pump, while still allowing the second to run when both floats are closed.

Must use the OT08PC socket for UL Rating!

  • Debounce time delay
  • Force lead pump operation when a pump is removed for repair or testing (on select models)
  • Force lead pump operation when a pump is removed for repair or testing (on select models)
  • Prevents nuisance actuating causes by waves or spashing in the tank
  • Force lead pump operation when a pump is removed for repair or testing (on select models)

ALT Alternating Relays Parts

FiltersFilters

Series: ALT Alternating Relays Resources