background-waves

Series: SE-COMM-RTD

Relay Interface Software
Product Status| Activei
info

This program is used to communicate with up to 63 SIO-RTD modules. It can be used to configure inputs on SIO-RTD modules as either 4-20mA or one of several RTD types. The data collected can be exported. The software has an autostart feature so that the program will restart when the computer reboots. SE-Comm-RTD now includes plotting for up to eight input signals.

SE-COMM-RTD Parts

FiltersFilters

Series: SE-COMM-RTD Resources